{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the Part Numbers of the I/O terminal blocks for the Momentum 170ADI54050?
Issue
What are the Part Numbers of the I/O terminal blocks for the  Modicon Momentum 170ADI54050 16 Point Discrete Input Module Base?

Product Line
Modicon Momentum I/O Base

Environment
Physical I/O connectors

Resolution
There are two I/O terminal block connectors (18pins) that are compatible with the 170ADI54050.
One is the screw-in type block with part number: 170XTS00100
The other is the spring-loaded type block with part number: 170XTS00200

Schneider Electric Nigeria