Issue
What does the TM2CSET terminal block connector set for Modicon M221 PLCs contain?
Product Line
Modicon M221 PLC
Environment
Physical connectors for wiring
Resolution
The TM2CSET terminal block connector set for the Modicon M221 I/O pins contains:
1x 8-pin screw connector terminal block
2x 10-pin screw connector terminal block
1x 12-pin screw connector terminal block
1x 13-pin screw connector terminal block
3x 9-pin screw connector terminal block
One set will include enough connector blocks of each type for each model of Modicon M221 PLC.
Released for:Schneider Electric Nigeria