Issue:
Program the ATV340 for 2-wire control
Product Line:
ATV340, Altivar 340
Environment:
All
Cause:
NA
Resolution:
From Main menu:
If desired, set 2-wire Type to Level instead of Transition control.
Warning: Level control type is not appropriate for all applications. Please consider whether this is safe for your application.
-In transition mode, the drive will need to be powered up before a run command is given.
-In level mode, the run command can remain active, and the drive will run upon power up.
If the run command is not active, the drive will wait for one in RDY status.
Program the ATV340 for 2-wire control
Product Line:
ATV340, Altivar 340
Environment:
All
Cause:
NA
Resolution:
From Main menu:
- Go to Complete Settings and enter.
- Go down to Command and Reference and enter.
- Go down to 2/3-wire Control and enter.
- Set for 2-wire control.
If desired, set 2-wire Type to Level instead of Transition control.
Warning: Level control type is not appropriate for all applications. Please consider whether this is safe for your application.
-In transition mode, the drive will need to be powered up before a run command is given.
-In level mode, the run command can remain active, and the drive will run upon power up.
If the run command is not active, the drive will wait for one in RDY status.
Released for:Schneider Electric Nigeria