{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause a buF [DB unit sh. circuit] fault on an ATV340 series drive and how do I correct it?
Issue:
Customer is experiencing BUF [DB unit sh. circuit] Fault on an ATV340 series drive.

Product Line:
ATV340

Environment:
External Braking resistor is being used.

Cause:
Short-circuit from braking circuit.

Resolution:
This fault appears when there is a short-circuit on the output of the braking transistor (desaturation of the braking IGBT).

Verify the wiring of the braking unit.
Verify that the braking unit value is not too low.

Schneider Electric Nigeria