{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the ATV320 obsolete?
Issue:
ATV320 obsolescence

Product Line:
Altivar 320

Environment:
All model numbers, all serial numbers

Cause:
Obsolescence documentation

Resolution:
The ATV320 is not obsolete.
It is a currently marketed product line, introduced in 2016.
The ATV320 is the functional replacement for the ATV32 and the ATV312, both obsoleted in 2017.

updated Feb 2022


Schneider Electric Nigeria