{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to send only one ingredient update to the PLC from a recipe in Vijeo Designer?
Issue:
Is it possible to send only one ingredient update to the PLC from a recipe in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
No, in Vijeo Designer, when you have multiple ingredients defined in a single recipe, you cannot send only one to the PLC. The Send operation will send all the recipe values to the PLC at once. If you need to send ingredient values one at a time, then it is suggested to make a recipe with only one ingredient variable.

Schneider Electric Nigeria