{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an INF8 [Internal Error 8] on an ATV340 series drive and how do I correct it?
Issue:
Customer is experiencing an INF8 [Internal Error 8] fault on an ATV340 series drive.

Product Line:
ATV340

Environment:
All

Cause:
The internal power switching supply is not correct.

Resolution:
Cycle power on the drive, this may clear the fault but the fault could return.  If the fault returns, contact your local Schneider Electric representative.

Schneider Electric Nigeria