Search FAQs
In SoMove why is the fast scope type not available when working with an ATV12?
Issue:
Why in the ATV12 is the fast scope type not available when working with SoMove?
Product Line:
Altivar 12
Environment:
SoMove commissioning software
Cause:
Fast scope selection is grayed out, not selectable
Resolution:
ATV12 is a basic drive and does not have Fast Scope function implemented.
Why in the ATV12 is the fast scope type not available when working with SoMove?
Product Line:
Altivar 12
Environment:
SoMove commissioning software
Cause:
Fast scope selection is grayed out, not selectable
Resolution:
ATV12 is a basic drive and does not have Fast Scope function implemented.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: