Search FAQs
How to remotely control (open/close) circuit breakers using IFE switchboard server and a browser. Discovering devices, creating a device list and enabling application control.
Issue:
This FAQ focuses in on the IFE switchboard server setup to remotely control open and close a circuit breaker using the embedded webpage, Powerview. Namely how to discover devices, create a device list and how to enable application control. However, one of the attachments is an example of what other components are needed, like MX-Com and XF-Com communicating coils, BCM, IFE Server, how to wire the communications coils etc.
Product Line:
Circuit Breakers
Environment:
Masterpact NT, NW and MTZ
Resolution:
This FAQ focuses in on the IFE switchboard server setup to remotely control open and close a circuit breaker using the embedded webpage, Powerview. Namely how to discover devices, create a device list and how to enable application control. However, one of the attachments is an example of what other components are needed, like MX-Com and XF-Com communicating coils, BCM, IFE Server, how to wire the communications coils etc.
Product Line:
Circuit Breakers
Environment:
Masterpact NT, NW and MTZ
Resolution:
Summary of Activity:
• Install MX-COM and XF-COM coils
• Install communications wire harness between coils and BCM
• Modify MX-COM and XF-COM input power wiring
• Install one IFE switchboard Server in place of one existing standard IFE, or add the IFE switchboard server in the ethernet daisy change with the IFE's
• Configure IFE switchboard server, namely discovering devices, creating a device list and enabling application control
See attached documents for example diagrams and specific instructions on how to discover devices, create a device list and how to enable application control.
See attached documents for example diagrams and specific instructions on how to discover devices, create a device list and how to enable application control.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: