{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why TesysT logic inputs are unexpectedly activated if nobody activated pushbutton connected to logic input?

It can happen due to very long cables connected to a logic input. This problem is more frequent in the case of AC signal than DC signal. Long cables (over 50m) have a capacitance that is significant enough for flowing the leakage current that can unintentionally activate TEsysT logic input.
Solution:
Use shorter cables
Use LTMR...BD instead of LTMR..FM. DC signal has a lower leakage current than AC.
Use interposing relay. The coil of the interposing relay has a lower impedance than the TEsysT logic input and so a greater current in the connected signal cable is needed to energize the relay. A push button installed far away will activate the relay (the relay must be close to TEsysT) and contact from the relay will activate LTMR logic input.
Add a resistor to each LTMR logic input.

Schneider Electric Nigeria

Attachment(s)

Special_case_Long_lines_AC.pdfSpecial_case_Long_lines_AC.pdf [642.13 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: