{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why the pdf printing report is not working anymore with Ecostruxure Machine Scada Export v8.1 SP2?
With Ecostruxure Machine Scada Export v8.1 SP2, the feature "PDF print report" is not working anymore, only rtf file are generated, not a pdf
To fix the issue a HF is available
The HF can be downloaded using this link: https://schneider-electric.box.com/s/hfe8nnwm4jlnk5ra2bmid3din7ck5f2j

In oder to install the HF, please follow the following step
- Close Ecostruxure Machine Scade Expert, stop the runtime if it’s running.
- Unzip the folder and put all its content (the dll and exe files) inside of the product installation Bin folder replacing the original ones: C:\Program Files (x86)\Schneider Electric\Ecostruxure Machine Scada Expert v8.1\Bin
- Open a command prompt as administrator (cmd.exe -> right click -> run as administrator) and execute this command: regsvr32 “C:\Program Files (x86)\Schneider Electric\Ecostruxure Machine Scada Expert v8.1\Bin\ISSymbol.ocx”
Please double check that the EMSE installation path is the good one.
You should have this following message to confirm that the HF has been correctly installed

Now the function pdf print report is working well!

Schneider Electric Nigeria