{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
For the Modicon M241 and M251 PLC, is there a method of changing the Modbus Ethernet port number from the standard 502?
Issue
For the Modicon M241 and M251 PLC, is there a method of changing the Modbus Ethernet port number from the standard 502?

Product Line
Modicon 241, M251
EcoStruxure Machine Expert v1.2
EcoStruxure Machine Expert v2.0
SoMachine v4.3

Environment
PLC Modbus Ethernet communication

Resolution
For the Modicon M241 and M251 the method of changing the Modbus TCP Port from the default 502 is done via a script command from SD Card using the "changeModbusPort" command.
For instructions, see the M241 or M251 Programming Guide under the help section:
> Ethernet Configuration > Ethernet Features, Functions and Services > Changing the Modbus TCP Port

M241 Changing the Modbus TCP Port Link to Manual
M251 Changing the Modbus TCP Port Link to Manual

Note: For other PLC families in SoMachine v4.3 and EcoStruxure Machine Expert v1.2 / v2.0 (Modicon M258, M262, HMISCU, LMC058, PacDrive 3), the above method is not supported.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: