{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Where do I enter motor information for a synchronous motor on an ATV320 Series Drive?

Article available in these languages: Japanese

Issue:
Customer needs to program an ATV320 series drive with motor information from a synchronous motor

Product Line:
ATV320 series

Environment:
Synchronous motor is being used.

Cause:
N/A

Resolution:
The ATV320 series drive has a separate menu for synchronous motors and asynchronous motors.
For Synchronous motors, navigate from RDY -> CONF -> Full -> DRC-  -> SYN- .  Motor nameplate information can be entered here.
For Asynchronous motors, navigate from RDY -> CONF -> Full -> DRC- -> ASY- .

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: