Issue:
ATV320 with Synchronous reluctance motors.
Product Line:
ATV320
Environment:
All model numbers, all serial numbers
Cause:
NA
Resolution:
No, the ATV320 is not designed for reluctance type synchronous motors. Only ATV600/900 series and ATV340 drives can be used with reluctance motors. These drives have the control law dedicated to run this kind of motor.
ATV320 with Synchronous reluctance motors.
Product Line:
ATV320
Environment:
All model numbers, all serial numbers
Cause:
NA
Resolution:
No, the ATV320 is not designed for reluctance type synchronous motors. Only ATV600/900 series and ATV340 drives can be used with reluctance motors. These drives have the control law dedicated to run this kind of motor.
Released for:Schneider Electric Nigeria