{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does BMXDAO1615 module have internally connected pins on the module connection?
Issue:
Customer wants to know on BMX DAO1615, any one of the pins between C3/C3, C7/C7, C11/C11, and C15/C15 can be used for the wiring.

Product Line:
x80 DAO module

Environment:
All

Resolution:
Yes. Pins (8,10) C3, Pins (18,20) C7, Pins (28,30) C11 and Pins (38,40) C15 are internally connected.

Schneider Electric Nigeria

Attachment(s)
Module Connection.7z [61 KB]