{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the torque specification for the bolts that attach the bolt-down bracket to the NetShelter cabinet?
Issue:
A customer wants to make sure they have the correct torque for the bolts that attach a bolt-down bracket to the NetShelter cabinet.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customer is asking for torque spec for the bolts of a bolt-down bracket.

Resolution:

To connect a bolt-down bracket to the NetShelter SX cabinet please use 80 - 100 lb-in. (9 - 11.3 N*m).
To connect a bolt-down bracket to a floor anchor please use the torque specified by the floor bolt manufacturer.

Schneider Electric Nigeria