Issue:
Programming & Wiring an E-Stop for the ATV212.
Product Line:
ATV212
Environment:
All model numbers, all serial numbers
Cause:
n/a
Resolution:
Consider using a logic input that is assigned as run permissive. If the input drops out, the VFD will remove output power to the motor.
Wire the normally closed E-stop contact between R and P24.
Program F110 = 0, F112 = 1.
The VFD will display OFF to indicate that a run permissive is not enabled.
Programming & Wiring an E-Stop for the ATV212.
Product Line:
ATV212
Environment:
All model numbers, all serial numbers
Cause:
n/a
Resolution:
Consider using a logic input that is assigned as run permissive. If the input drops out, the VFD will remove output power to the motor.
Wire the normally closed E-stop contact between R and P24.
Program F110 = 0, F112 = 1.
The VFD will display OFF to indicate that a run permissive is not enabled.
Released for:Schneider Electric Nigeria