Search FAQs
How can I mount the VW3A1101 keypad further than 30 feet away from an Altivar Drives?
Issue:
Customer needs to mount the VW3A1101 keypad further than the recommended 30 feet away from the drive.
Product line:
VW3A1101 keypad and all drives it is used with.
Environment:
All models and serial numbers
Cause:
Non-standard installation. The maximum recommended distance using our supplied cables is 30 feet.
Resolution:
Please see attached drawing. It will be necessary to add in a splitter, coupler, and external 10VDC power supply capable of 100ma of current or greater. These are generic parts that are widely available.
Customer needs to mount the VW3A1101 keypad further than the recommended 30 feet away from the drive.
Product line:
VW3A1101 keypad and all drives it is used with.
Environment:
All models and serial numbers
Cause:
Non-standard installation. The maximum recommended distance using our supplied cables is 30 feet.
Resolution:
Please see attached drawing. It will be necessary to add in a splitter, coupler, and external 10VDC power supply capable of 100ma of current or greater. These are generic parts that are widely available.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: