{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Prisma P dedicated cubicles for Masterpact can be designed with the horizontal busbar connections installed at the bottom and the cable connections at the top of the panel?
The Prisma P dedicated cubicles for Masterpact circuit breakers can be designed with the incoming and outgoing connections opposite from the model shown in the product catalog. The busbar connection may be installed at the bottom of the switchboard and the terminal extension bars for cable connection at the top.

The same busbar connections may be used.

Please consider that the vertical distances may have to be adapted depending on the position of the breaker in the cubicle (distance from the terminals to the horizontal busbar).

When horizontal busbars are at the bottom of the cubicle, gland plates are mandatory at the bottom of the cubicle.

Schneider Electric Nigeria