{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What causes an OHF Overheating fault on the ATV320 drives?
Issue:
ATV320 with Overheating Fault OHF.

Product Line:
Altivar 320, Machine Drives

Environment:
All

Cause:
Over heating

Resolution:
OHF [Drive overheat] • Drive temperature too high. • Check the motor load, the drive ventilation and the ambient temperature. Wait for the drive to cool down before restarting. Check to see if the fans are running.  Drive thermal state of 70% and above should allow the fans to come on.  Under monitoring NON- menu. THd [Drv.thermal state] % Drive thermal state.  100% = Nominal thermal state, 118% = "OHF" threshold (drive overload).

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Nigeria