{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many built-in RJ45 communication ports are in an ATV630 drive?
Issue:
Number of RJ45 communication ports on a standard ATV630 drive

Product Line:
ATV630

Environment:
All serial numbers

Cause:
Customer wanted to know how many serial ports comes with the ATV630 drive.

Resolution:
The ATV630 has 2 built-in RJ45 communication ports as standard:
1 Ethernet Port (TCP only)
1 Modbus Serial Port

Schneider Electric Nigeria