{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
what is the reason of Reset Reason 8 in Scada pack ER Magna RTU ?
A reset reason of 8, simply means that someone or some code triggered the SCADAPack to restart. You can do this in Configurator by selecting the dropdown menu "Commands -> Restart RTU ...". It can also be performed via command line interface by typing "Restart RTU"

If a user wanted to program the SCADApack to do this in logic it could also be possible with the "cmd_exec" function block, where the block has the input iCmd as 'Restart RTU".

ClearSCADA can also issue commands like this.

Schneider Electric Nigeria