{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Why in Ecostruxure Secure Connect Advisor, some agent are visible in Gatemanager even if there are not connected physically?
1. Issue
When the SiteManager is installed on HMIGTO or HMIG3U, all agents are visible event if there are not physically connected to the SiteManeger. There are visible in GateManager, LinkManager and they reply "present" to ping command

2. Product Line
Ecostruxure Secure connect Advisor

3. Environment
When the Site Manager of Ecostruxure Secure connect Advisor is installed on VxWord target (HMIGTO, HMIG3U)

4. Resolution
For a diagnostic, if SiteManager is on HMIGTO/HMIG3U, do not use Ping command to check if your agents are connected or not

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.