{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an INF4 fault on the ATV61 and ATV71 drives?
Issue:
INF4 fault on the ATV61 and ATV71.

Product Line:
ATV61 and ATV71 drives

Environment:
All

Cause:
INF4 is an Internal Zone Fabrication Error which is caused by incoherent internal data on the EEPROM.

Resolution:
* Recalibrating the drive using the diagnostic menu. (This option is only available for the field services techs)
* Change the control bloc or power board.

Schneider Electric Nigeria