{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to update price list in Ecostruxure Power Build - Rapsody?

Article available in these languages: Russian

Issue: How to update the pricelist in Ecostruxure Power Build-Rapsody.
Product Line: Ecostruxure Power Build – Rapsody
Resolution:
Requirement of pricelist file:

1. Identifying file:
The file format should be *.TXT

2.  Building the file:
The file has two columns: First with part number & second with prices
In this example below, the price of ref 'ALB71338' is 17.44 (the decimal is automatically inserted before the last 2 digit)



3-Completion of the file:
File must begin with 3 lines: @Comment, @currency and @date, as shown in the above snapshot

Warning: the format of date must be dd.mm.yyyy

Once you have the pricelist file available with you, follow the below steps to update the pricelist in Rapsody software.

Step1: Click on the Tools option from top right side on the EPB Rapsody software and select the option “Update prices” (as shown in below screenshot)


Step2: In Update Prices window, under New price update, use the folder icon to navigate and select the .txt pricelist file from local computer and click ok





Step3: After successful completion of pricelist update, In Switchboard tab we can see the Current Pricelist (as shown below)

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.