{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to setup VIA and VIB on the ATV212 drive using 0-5V instead of 0-10V?

Issue:
Can I set 0-5V analog signal on VIA and VIB on the ATV212 drive?

Product Line:
Altivar Machines, Altivar 212, S-Flex

Environment:
All model numbers, all serial numbers

Cause:
Customer wanted to use 0-5V instead of 0-10V.

Resolution:
For setting up VIA using 0-5V, then follow the steps below:
F201 = 0
F202 = 0
F203 = 50% or 5V
F204 = 60 for 60Hz in US

For setting up VIB using 0-5V, then follow the steps below:
F210 = 0
F211 = 0
F212 = 50% or 5V
F213 = 60 for 60Hz in US

In addition, please make sure SW100 (voltage/current selection for analog I/O VIA and VIB) are set for U (voltage).


Schneider Electric Nigeria