{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Altistart 48 use Fast acting fuses on the line power?

Issue:
Fact acting fuses protecting the ATS48

Product line:
Altistart 48 softstart controller

Environment:
all

Cause:
Documentation does not show fact acting

Resolution:
Fast acting fuses are not recommended.  The starting currents on a soft start can be upwards of 400% or more of motor FLA for the duration of the ramp to full speed.  It is recommended to use time delay fuses only.

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.