{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is Form Y190 for the 8940 Pump Panels?
Issue:
8940 modifications

Product Line:
Class 8940, Well-Guard Control™ Pump Panels

Environment:
Full Voltage, Type SS, XS

Resolution:
Form Y190 is only available on the Class 8940 Pump panels.  This is to remove the existing Type S contactor and replace with 8502W vacuum contactors.

Schneider Electric Nigeria