Graphical display for ATV71 is not compatible with ATV340.
Graphic keypad (VW3A1101) is compatible with Altivar 312 ,Altivar 61, Altivar 71, Altivar 32, Altivar 212, Altivar Lift, Altivar 61Q, Altivar 71Q, Altivar 312 Solar and Altivar Machine ATV320.
Another type of graphic keypad (VW3A1111) is used with ATV340 which is compatible also to Altivar process drives (600 and 900).
Graphic keypad (VW3A1101) is compatible with Altivar 312 ,Altivar 61, Altivar 71, Altivar 32, Altivar 212, Altivar Lift, Altivar 61Q, Altivar 71Q, Altivar 312 Solar and Altivar Machine ATV320.
Another type of graphic keypad (VW3A1111) is used with ATV340 which is compatible also to Altivar process drives (600 and 900).
Released for:Schneider Electric Nigeria