What is the maximum voltage per pole for iC60, C120, NG125 and C60H-DC?
The C60 (or iC60) offers are compliant with 60V DC per pole. C120 / NG125 offers are compliant with 125V DC by pole C60H-DC offer is compliant with 250V per pole.
Released for:Schneider Electric Nigeria
Explore more
Range:
C60H-DC
Acti9 iC60
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.