{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for the XBTF024110 Magelis HMI?

Article available in these languages: Spanish

Issue:
Replacement model for the XBT-F024 series Magelis HMI (XBTF024110, XBTF024310, and XBTF024510)


Product Line:
Vijeo Designer, XBTF, XBTL1000, HMIGK


Resolution:
The replacement for the XBT-F024 model series HMI (including part numbers XBTF024110, XBTF024310 and XBTF024510) is the
HMIGK5310. The HMIGK5310 is programmed using Vijeo Designer V6.2 development software. The XBTF project must be converted to Vijeo Designer either manually or via the Schneider Electric Industrial Automation Tech Support.

Schneider Electric Nigeria