{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can X80 modules that start with BME- be used with M340?
Issue:
I am configuring my M340 in Control Expert and unable to select modules that begin with the BME- prefix such as BME NOC 03X1, BME NOP 0300, BME NOS 0300, BME AHI 0812.
I am also unable to select any of the partner modules such as the PME SWT 0100.
Why can't these modules be used with the M340?

Product Line:
M340, M580, X80, BMX, BME

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
The X80 IO and Communication modules that start with the BME- or PME- prefix require the use of the dual X-bus and Ethernet portions of the BME backplanes.
Therefore, these modules are only compatible with the M580 CPUs and not M340.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria