{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to connect to ATV 2*3 PTCs if they are connected in start? There are 3 branches with 2xPTC in series. 3 branches are connected to star. Outputs are 3 endpoints and star point
Depending on ATV type, for example ATV6000, ATV630, ATV930 allows connection of min 1 and max 6 PTC connected in series.
I this case with 6PTC if they are connected in star like:
EP1-PTC1-PTC2-STAR,
EP2-PTC3-PTC4-STAR,
EP3-PTC5-PTC6-STAR
EP means endpoint),

then only 4 PTCs can be connected: ATV(AIx)-EP1-PTC1-PTC2-PTC4-PTC3-EP2-ATV(COM). Star point and third rung with EP3 will remain not connected.

Schneider Electric Nigeria