Search FAQs
What is the maximum number of I/O objects that the TM3BCEIP can support?
Issue
Up to how many I/O objects can the TM3BCEIP Bus Coupler have?
Product Line
Modicon TM3
Environment
Distributed I/O Modules for M221, M241, M251, M262
Resolution
The TM3BCEIP Bus Coupler for Ethernet/IP and Modbus TCP has the capability of adding 14 (TM3) I/O nodes with a maximum of 64 WORDs for Inputs and 64 WORDs for Outputs (each WORD being 16-bits).
Up to how many I/O objects can the TM3BCEIP Bus Coupler have?
Product Line
Modicon TM3
Environment
Distributed I/O Modules for M221, M241, M251, M262
Resolution
The TM3BCEIP Bus Coupler for Ethernet/IP and Modbus TCP has the capability of adding 14 (TM3) I/O nodes with a maximum of 64 WORDs for Inputs and 64 WORDs for Outputs (each WORD being 16-bits).
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: