{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a Trial version for EcoStruxure Machine SCADA Expert v8.1?
Issue
Where can I find a Trial version of EcoStruxure Machine SCADA Expert v8.1 for download?

Product Line
EcoStruxure Machine SCADA Expert

Environment
HMI/SCADA Configuration software for Windows

Resolution
Yes, there is a Trial version of EcoStruxure Machine SCADA Expert v8.1.
The latest version for v8.1 as of December 19, 2019 is v8.1 SP5.
The version which supersedes v8.1 is v2020.

The download can be obtained with this link:
https://www.se.com/ww/en/download/document/Machine_SCADA_Expert_v8.1_SP5/

For v2020 or the latest version, go to:
https://www.se.com/ww/en/product-range/63734-ecostruxure%E2%84%A2-machine-scada-expert/#software-and-firmware

The Editor (Configuration Software) Trial will run for 40 hours of use.
The Runtime (HMI) will run for two hours at a time.

If you wish to have your PC run as a webserver, please activate Windows Internet Information Services (IIS) from Programs and Features before installation

Schneider Electric Nigeria