{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert - Why Trend report saved in pdf format, includes a number of blank pages?
Issue
A Trend report is configured, generated, and then dowloaded as a pdf file. The pdf file includes a number of blank pages.

Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
Web Applications - Reports

Cause
When a Trend report is configured to include a large number of measurements, if that report is downloaded in pdf format it will include a number of blank pages. This happens because of the way the reporting services handles wide tables. In the Trend report only graph is visible, but the blank pages get added to match the width of the table expansion even though the table is not visible.

Resolution
The known workaround is to limit the number of measurements to from one to six when configuring the report, to keep the tables smaller in width.

Schneider Electric Nigeria