{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION7650/7550 with current probe phase angle for current does not change after applying calibration constants
Issue
After changing the calibration constants of the current probe in the ION meter using terminal access and command kctstp, the meter's phase angle for current does not change

Product
ION 7650
ION 7550

Environment
ION Setup
Front panel
Power Monitoring Expert

Cause
The phase angle correction is only applied to the kW, kVA, kVAR in the power meter module only

Resolution
Phase angle adjustments are used for power correction only.

Schneider Electric Nigeria