Search FAQs
Can a NetBotz Door Switch Sensor be installed onto NetShelter SX with RACS?
Issue:
There are no holes in the Rack Air Containment frame (front or rear) for the NetBotz Door Switch Sensor install onto.
Product Line:
NetBotz NBES0301, NBES0302
HACS ACCS1006, ACCS1007
Environment:
All versions and serial ranges.
Cause:
The frame of the Rack Air Containment does not include the pre-drilled holes for NetBotz that the NetShelter SX does.
Resolution:
The NetBotz Door Switch Sensors can be installed using the included 2-sided tape. Please see the attached document.
There are no holes in the Rack Air Containment frame (front or rear) for the NetBotz Door Switch Sensor install onto.
Product Line:
NetBotz NBES0301, NBES0302
HACS ACCS1006, ACCS1007
Environment:
All versions and serial ranges.
Cause:
The frame of the Rack Air Containment does not include the pre-drilled holes for NetBotz that the NetShelter SX does.
Resolution:
The NetBotz Door Switch Sensors can be installed using the included 2-sided tape. Please see the attached document.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: