{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an alternative part for the HMIZGAUX?
Issue:
The lead time for the HMIZGAUX is quite substantial. Looking for an alternative part number for the same part.

Product Line:
Magelis HMI (XBTGT, HMIG3U, HMIG3X, HMIG5U, HMIG5U2)

Resolution:
If the lead time for the HMIZGAUX is too long, consider checking your suppliers for Phoenix Contact's equivalent part of: FK-MC 0.5-2.5 7 position. (1908114)

Schneider Electric Nigeria