{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does the PME base license come with an engineering client license?

Issue
The PME 9.0 and newer System Guides state that "the base license includes one engineering tools feature," but it does not define whether this engineering tool can be used on the server and a client machine.

Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Licensing

Resolution
Engineering tools license can be used by a client machine or the server as long as it is not concurrent.

For example, 1 engineering tools license can connect from the client, if it's not currently used anywhere else. After the client closes the connection, a connection can be made from the server or another client machine.

Note: The only exception is that the trial license is locked to the server. Which means that a system with only the trial license would only be able to connect from the server.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: