{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the vertical installation supported for EcoStruxure Building Operation Automation Server (AS/AS-P/AS-B)?
Always install (AS, AS-P, AS-B, I/O modules, and PS-24) on a horizontal DIN rail. This position provides sufficient cooling airflow through the device. Installation on a vertical DIN rail can reduce
the life span of the device.
AS/AS-P:

AS-B:

Schneider Electric Nigeria