{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to sync the alarm status in two HMIs

  1. Issue
How to sync the alarm status (Active,Acknowledge,,Gone) in two HMI Targets.
  1. Environment
Vijeo Designer 6.2 [SPx].
  1. Resolution
User can use Data Sharing and RemoteCategory to sync the alarm status in different HMI Targets. Here is an example.
Step 1. Add 2 Targets in VJD project and enable Data Sharing.



Step 2.In Target1,create an Alarmgroup and select Read/Write in the setting.

Step 3.In Target2,create a RemoteCategory and select Alarmgroup1 in the setting.


Step 4.Add Alarm Summary in Graphical Panel in Target1,select Alarmgroup1 in Alarm Summary Settings.

Step 5.Add Alarm Summary in Graphical Panel in Target2,select RemoteCategory1 in Alarm Summary Settings.

Step 6. Download Projects to HMI Targets, loop HMI Targets in the same network, user will get the same alarm status (Active,acknowledge,,gone) in both of these 2 HMI Targets.
  1. FAQ Applicable Conditions
FAQ applies to all Vijeo Designer 6.2 SPx.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: