{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why breaker for ATV340 D22N4 is bigger than for D30N4E?

From 30kw and above, the ATV340 has the same hardware as ATV930. It means it has also dc choke.

ATV340 of 22kW and below are different. That is why 30kW drive ATV340 has lower input current and lower contactor and breaker needed than 22kW drive (with more harmonics).

Schneider Electric Nigeria