Customer cannot add a custom library by using Types Library Manager in Unity Pro V13.1
Issue
Customer cannot add a custom library by using Types Library Manager in Unity Pro V13. However, customer can add a custom library if the Libset version is set to V12, not V13.1. Customer also has full admin rights on the PC and VM. Reinstalling the Unity Pro doesn’t work as well.
Product Line
Unity Pro V13.1
Environment
Unity Pro V13.1, Win10
Resolution
Manually replacing the custom.db file of V13.1 can fix the issue. The root cause is the custom.db file is corrupted due to the installation package of Unity Pro which has potential error.
Released for:Schneider Electric Nigeria
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.