In a virtual machine, user is able to see PLC M241 but not HMISCU via USB cable in SoMachine V4.3, how to fix the issue? VMware and SoMachine V4.3.
Normally it is caused by the USB compatibility setting in Virtual Machine, user can change the setting from USB 3.0 to USB 2.0, then the HMISCU Target can be detected in SoMachine V4.3.

Normally it is caused by the USB compatibility setting in Virtual Machine, user can change the setting from USB 3.0 to USB 2.0, then the HMISCU Target can be detected in SoMachine V4.3.
Released for:Schneider Electric Nigeria