{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I add a delay timer on each ATS01 soft starter to avoid overloading the pumps?

Issue:
Can I set up a timer to start three soft starters in sequence?

Product Line:
Altistart ATS01

Environment:
All model numbers

Cause:
Customer want to start each soft starter in sequence using a timer delay.

Resolution:
Customer has to use external controls because it is not a feature of ATS01.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: