{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the ENM Tool installation file in PME 2020? Does it need a separate license?
Product Line
Event Notification Module(ENM) in Power Monitoring Expert (PME) 2020

Environment
PME 2020, Event Notification Module(ENM)

Cause
The ENM installer does not exist in the same location of the PME .iso that it did in previous versions.

Resolution
In PME 2020, the Event Notification Module has been completely redesigned. ENM now includes a new notification engine that seamlessly integrates with PME for alarm-based notification, so there is no separate ENM installation file.

ENM is a built-in feature of PME. It is available for configuration as soon as the ENM license has been activated. Therefore a separate Base License is required.

Note: You can open Notifications from Settings > Alarms  >Notifications in Web Application.

Schneider Electric Nigeria