{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can't I assign a digital input to Command and Reference switching on ATV630?
Issue:
Why can't I assign 2 compatible functions to the same digital input?

Product Line:
ATV630, ATV660 , ATV650

Environment:
All serial numbers ,

Cause:
Programming Hand Off Auto functionality

Resolution:
Need to verify that the Access Level is set to Expert. Then you can assign 2 different functions to the same digital input.

Schneider Electric Nigeria