Search FAQs
What are the recommended replacement parts for the ION7650 series meter and PowerLogic Circuit Monitor CM4000T meter?
Product Line
PowerLogic Circuit Monitor CM4000T meter
ION7650 series meter
ION9000(T) series meter
Environment
End of commercialization and recommended replacement
Cause
The ION7650 series meter and the CM4000T meter are obsolete.
Resolution
ION7650
The recommended replacement for the ION7650 is the ION9000 series meter. The meters are not physically identical. The ION7650 series also had Ethernet Fiber capability. This feature is not enabled on the ION9000.
The ION9000 can be ordered with or without the remote display:
CM4000T
The recommended replacement for the CM4000T is the ION9000T series meter.
The ION9000T can be ordered with or without the remote display:
See the following links and attached pdfs for documentation on all the meters, including the comparison table to view the differences:
PowerLogic Circuit Monitor CM4000T meter
ION7650 series meter
ION9000(T) series meter
Environment
End of commercialization and recommended replacement
Cause
The ION7650 series meter and the CM4000T meter are obsolete.
Resolution
ION7650
The recommended replacement for the ION7650 is the ION9000 series meter. The meters are not physically identical. The ION7650 series also had Ethernet Fiber capability. This feature is not enabled on the ION9000.
The ION9000 can be ordered with or without the remote display:
- Without display: METSEION92030
- With display: METSEION92040
CM4000T
The recommended replacement for the CM4000T is the ION9000T series meter.
The ION9000T can be ordered with or without the remote display:
- Without display: METSEION95030
- With display: METSEION95040
See the following links and attached pdfs for documentation on all the meters, including the comparison table to view the differences:
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: