{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
HVAC valve and actuator selection
"Valve and Actuator Selection tool" is publicly available webtool that can be used desktop computers as well as mobile devices 10” or larger, with the latest browsers and their updates applied. It is designed to simplify the process of selecting and scheduling Schneider Electric Valves/Assemblies and Damper Actuators. This tool quickly and easily puts a wealth of information at the user’s fingertips to ensure specification of the optimum Schneider Electric part to fit their application.

Many of the new and enhanced features of the tool enable users to:
  • Save and load customer profiles
  • Schedule hydronic systems using the Valve Assembly selection feature
  • Schedule damper applications using the Damper Actuator selection feature
  • View, edit, change and adjust schedules
  • Download schedules to Excel or as a pdf or BOM.
  • Save in-progress schedules so you can work on them later, or use as a template for future projects

Schneider Electric Nigeria